{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to have the NetShelter SX side panels open using the same key as the AR8132A?
Issue:
The AR8132A key will not lock or unlock the NetShelter SX side panels.

Product Line:
NetShelter SX, Colo

Environment:
All versions and serial ranges.

Cause:
The side panel uses a #333 key, but the AR8132A uses a #222 key.

Resolution:

The lock cylinders on the NetShelter SX side panels can be changed to match the key of the AR8132A.
To do so, please see FAQ FA158606: https://www.apc.com/us/en/faqs/FA158606/ This document will help you understand the different lock options available, and how to source them.

Schneider Electric Saudi Arabia