{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the RM35JA31MW monitor positive and negative currents?
Issue:
Checking if Zelio relays can monitor negative currents.

Product line:
Relays and Timers

Environment:
Zelio Control and Measurement Relays

Cause:
Documentation shows on 4-20mA does not clarify positive or negative.

Resolution:
Yes, the RM35JA31MW can monitor +4 to +20mA or -4 to -20mA.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.