{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the HMISCU Control Application be used as a Modbus TCP Server?

Issue
I want to use the HMISCU Control Application as a Modbus TCP Server so that another PLC can read/write to its Modbus registers. Is this possible?

Product Line
Magelis SCU (HMISCU), SoMachine / EcoStruxure Machine Expert

Environment
SoMachine / EcoStruxure Machine Expert configuration software

Resolution
Yes, the HMISCU's Control (PLC) Application can be used as a Modbus TCP Server.
The HMISCU supports a Library from 3S called "ModbusTCP Slave", which contains a function block named "ModbusServer" (also known as "MTS.ModbusServer"). This Modbus server is managed by the IEC controller application.

In the attached ZIP "FA379937 HMISCU ModbusServer Guide and Example.zip" there are two files:

1) See the guide written in MS Word on how to implement the function block.
Filename: "Modbus TCP Server for HMISCU Control Application Guide.doc"

2) Also see the sample project which uses the HMISCU as a Modbus TCP Server and an M251 as a Client (polling with the Modbus IO Scanner feature). This project was written in SoMachine v4.1 SP1 (and can be opened in any newer version of SoMachine / EcoStruxure Machine Expert Basic).
Filename: "MBserverFB HMISCU M251v4.1SP1_2.projectarchive"

Schneider Electric Saudi Arabia

Attachment(s)

FA379937 HMISCU ModbusServer Guide and Example.zipFA379937 HMISCU ModbusServer Guide and Example.zip [2.44 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: