{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In SE8600 series room controller, can cooling CPH be set to value higher than 4?
Cooling Output Cycles Per Hour "CPH" is used to “modulate” On/Off outputs controlling equipment such as compressors. When the Room Temperature is within the Proportional Band, the output performs 3 or 4 CPH. A higher CPH represents a higher accuracy of control at the expense of wearing mechanical components faster.
The CPH can value 3 or 4. you cannot set a higher value than 4 to cooling CHP. This is to protect the compressors from burning out due to cycling on and off. Even 4 cycles per hour are not recommended for some units.

Schneider Electric Saudi Arabia