Search FAQs
Does EcoStruxure Machine Expert support M258, LMC058 and LMC078 controllers?
Issue:
Some older versions of EcoStruxure Machine Expert versions do not have M258, LMC058 and LMC078 controllers on the list of available devices
Product Line:
M258, LMC058 and LMC078 controllers
Environment:
EcoStruxure Machine Expert versions 1.1, 1.2.x and 2.0 (formally known as SoMachine)
Resolution:
- EcoStruxure Machine Expert supports M258 and LMC058 controllers starting with version 1.2.5. Previous version of EcoStruxure Machine Expert did not support them.
- LMC078 controllers are not supported by any version of EcoStruxure Machine Expert. SoMachine 4.3 software should be used instead to program a LMC078 controller.
- EcoStruxure Machine Expert v2.0 will not support M258, LMC058 or LMC078 controllers anymore.
Some older versions of EcoStruxure Machine Expert versions do not have M258, LMC058 and LMC078 controllers on the list of available devices
Product Line:
M258, LMC058 and LMC078 controllers
Environment:
EcoStruxure Machine Expert versions 1.1, 1.2.x and 2.0 (formally known as SoMachine)
Resolution:
- EcoStruxure Machine Expert supports M258 and LMC058 controllers starting with version 1.2.5. Previous version of EcoStruxure Machine Expert did not support them.
- LMC078 controllers are not supported by any version of EcoStruxure Machine Expert. SoMachine 4.3 software should be used instead to program a LMC078 controller.
- EcoStruxure Machine Expert v2.0 will not support M258, LMC058 or LMC078 controllers anymore.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: