Search FAQs
Do we have Universal Socket Outlets? Are they compatible with DIN rail mounting?
Our Universal Socket Outlets can be found in the following ranges: Neo, ZENcelo, Pieno, Vivace, S-Classic and Lisse. However, these types are not compatible with DIN rail mounting.
The range that is compatible with DIN rail mounting is the iPC Modular Power Sockets range, but this range does not offer Universal Sockets. It only offers Schuko sockets as well as French and Italian type sockets. You can find the catalogue of the iPC Modular Power Sockets attached (CA904017E.pdf). You can also access the Wiring Devices catalogue through the following direct link: https://download.schneider-electric.com/files?&p_enDocType=Catalog&p_File_Name=Wiring%20Devices%20Catalogue%20%2718-LLR.pdf
The range that is compatible with DIN rail mounting is the iPC Modular Power Sockets range, but this range does not offer Universal Sockets. It only offers Schuko sockets as well as French and Italian type sockets. You can find the catalogue of the iPC Modular Power Sockets attached (CA904017E.pdf). You can also access the Wiring Devices catalogue through the following direct link: https://download.schneider-electric.com/files?&p_enDocType=Catalog&p_File_Name=Wiring%20Devices%20Catalogue%20%2718-LLR.pdf
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: