{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How many devices can control the Wiser for KNX device?

The Wiser for KNK (W4K) visualization is web based. So any device (connected to the same network as the W4K) having a web browser will be able to connect to the W4K IP address (default address: 192.168.0.10) and control the W4K. So many devices can login to the device and control it. Login credentials are illustrated in the attached instruction sheet (on the bottom left). At the same time, the User Manual of the W4K is provided in the attached link.

Schneider Electric Saudi Arabia

Attachment(s)

Wiser for KNX - User Guide 2018.pdfWiser for KNX - User Guide 2018.pdf [8.84 MB]
Wiser for KNX - Instruction Sheet.pdfWiser for KNX - Instruction Sheet.pdf [66.82 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: