Search FAQs
What are the technical details of the integrated optical transceiver of TCSESPU093F2CU0?
Issue
The TCSESPU093F2CU0 has two Multimode ports (type 50/125) and this FAQ gives the technical details of the integrated optical transceiver.
Product Line
ConneXium Switch
Environment
TCSESPU093F2CU0
Resolution
The TCSESPU093F2CU0 integrated optical transceiver has:
The TCSESPU093F2CU0 has two Multimode ports (type 50/125) and this FAQ gives the technical details of the integrated optical transceiver.
Product Line
ConneXium Switch
Environment
TCSESPU093F2CU0
Resolution
The TCSESPU093F2CU0 integrated optical transceiver has:
- Maximum optical power: -14dBm
- Transmit power: -23.5dBm
- Receiver sensitivity: -31dBm
- Loss budget: 7.5dBm
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: