{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 9.0 numeric objects scaled in Vista are not scaled on Web Applications
Issue
In PME 9.0, when scaling numeric object values in Vista using units starting with "G", "M", or "K", the value is scaled in Vista but not when the diagram is viewed in the Web Applications Diagrams tab.

Diagrams

Product Line
Power Monitoring Expert 9.0

Environment
Web Applications

Cause
This is a known issue in PME 9.0 that has been corrected in PME 9.0 CU1.

Resolution
Apply the latest PME 9.0 Cumulative Update (CU), which can be downloaded at Power Monitoring Expert 9.0 (se.com).

Schneider Electric Saudi Arabia