{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum number of I/O objects that the TM3BCEIP can support?

Issue
Up to how many I/O objects can the TM3BCEIP Bus Coupler have?

Product Line
Modicon TM3

Environment
Distributed I/O Modules for M221, M241, M251, M262

Resolution
The TM3BCEIP Bus Coupler for Ethernet/IP and Modbus TCP has the capability of adding 14 (TM3) I/O nodes with a maximum of 64 WORDs for Inputs and 64 WORDs for Outputs (each WORD being 16-bits).

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: