{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the leveling feet need to be used when installing a NetShelter SX cabinet per OSHPD or IBC High Seismic Area?
Issue:
Need to confirm proper installation per OSHPD and IBC High Seismic Area.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The NetShelter SX OSHPD and IBC Structural Calculations documents do not mention if the leveling feet must be down.

Resolution:

The calculations are all based on the anchorage points in the floor and the cabinet, but as in any installation it's always the best practice (recommended) to have the leveling feet down.
Please see the attachment for a good graphic representation of this question.

Schneider Electric Saudi Arabia

Attachment(s)
Does IBC High Seismic Area or OSHPD Require the use of Leveling Feet.pptx [149.73 KB]