{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a NetBotz Door Switch Sensor be installed onto NetShelter SX with RACS?

Issue:
There are no holes in the Rack Air Containment frame (front or rear) for the NetBotz Door Switch Sensor install onto.

Product Line:
NetBotz NBES0301, NBES0302
HACS ACCS1006, ACCS1007

Environment:
All versions and serial ranges.

Cause:
The frame of the Rack Air Containment does not include the pre-drilled holes for NetBotz that the NetShelter SX does.

Resolution:

The NetBotz Door Switch Sensors can be installed using the included 2-sided tape. Please see the attached document.

Schneider Electric Saudi Arabia

Attachment(s)

20191015 Mounting NetBotz Door Switch Sensors onto NetShelter SX with RACS.pdf20191015 Mounting NetBotz Door Switch Sensors onto NetShelter SX with RACS.pdf [1.26 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: