{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to wire a PTC probe to ATV320 drive?
Issue:
PTC probe wiring on ATV320 drive.

Product Line:
Altivar Machines, Altivar 320

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
DI6 can be used as PTC (Positive Temperature Coefficient) using SW2 switch (see page 89 of manual).
Trip threshold: 3 kΩ, reset threshold: 1.8 kΩ
Short-circuit detection threshold < 50 Ω
ATV320 PTC probe wiring.

PTC wiring
Wire the PTC to DI6 and COM.

Schneider Electric Saudi Arabia