{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In the NetShelter WX 6U Vertical cabinet, can the 2U UPS Mounting Bracket also be used on a 1U or 3U Smart-UPS?
Issue:
It is unknown whether a 1U ot 3U Smart-UPS can use the 2U mounting rail.

Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The AR106V And AR106VI comes with a 2U UPS mounting rail installed.

Resolution:

The UPS Mounting Bracket is made for a 2U APC Smart-UPS.
To mount a 1U or 3U Smart-UPS into the AR106V/VI please use the mounting rail kit that comes with the UPS.

Schneider Electric Saudi Arabia