{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 3rd party UPS be installed in the AR106V or AR106VI?
Issue:
It is unknown if a 3rd Party UPS can be installed into the AR106V and AR106VI.


Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS.

Resolution:

Any 3rd party UPS must be validated by the manufacturer to work with this cabinet prior to installation:
The manufacturer must validate that the 3rd party UPS can be installed vertically. Not all batteries can install in this orientation.
When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit.

Schneider Electric Saudi Arabia