{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to add PUC variable or other not-listed variable into ethernet scanner of ATV630, ATV930 or ATV340?
If the register name cannot be found in the list of variables, it can be added using its address.
In ethernet I/O scanner, when adding new variable, select the type of variable as logical address. Then enable searching in internal addresses. Choose the logical address you want to add and start searching.
The variable should appear in the list, so you can add it. See attached picture.
When it comes to PUC variable (not available in ATV630) , bear in mind that in latest fw of ATV930 and ATV340 there has been added new PUCD variable that carries the same type of information as PUC (counting pulses from encoder), but its range is 32-bit value.
PUC at address is 5611 is 16-bit value
PUCD at address 5668 is 32-bit value


Maybe you cannot find PUC in ethernet i/o scanner. That is true, by default it is not in the list. However its address can be added manually by selecting “logical address” and enabling “Internal addresses”, see attachment.
Bear in mind that in latest fw version of ATVs , there is also 32-bit values of PUC (called PUCD), address 5668.
Both PUC and PUCD are available in list of eth scanner when added manually, see picture.

Schneider Electric Saudi Arabia

Attachment(s)
How to add PUC or PUCD into ethernet scanner.jpg [302.09 KB]