{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the switching power of ATV process relay outputs?
This information can be found on product datasheet on web.

Max switching power for AC load is:
2A at 250V AC providing that the load is resistive or slightly inductive with either cos phi 0.4 or better or time constant L/R of 7ms or lower.
Max switching power for DC load is:
2A at 30V DC providing that the load is resistive or slightly inductive with either cos phi 0.4 or better or time constant L/R of 7ms or lower.

Schneider Electric Saudi Arabia

Attachment(s)
Relay.jpg [49.54 KB]