{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will it trigger the network storm by connecting the respective ctrl port of BMENOC0321 from HSBY system onto the same switch?
  1. Issue
When ip forwarding service is activated, the BMENOC0321 automatically enables its backplane port.
Then will it trigger the network storm by connecting the respective ctrl port of BMENOC0321s from HSBY system onto the same switch?
  1. Environment
N/A
  1. Resolution
No, it will not trigger the network storm by connecting the respective ctrl port of BMENOC0321s from HSBY system onto the same switch.
Although the backplane port is automatically enabled, the link between ctrl network and fieldbus network is isolated.
So it will not cause the unintentional ethernet loop in this loop.


Schneider Electric Saudi Arabia