Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why a 4-20 mA is preferred to 0-10V in analog signals?
The bottom span 4 mA expresses a minimum signal value than a broken wire.
Since the loop current never falls to zero, it can be loop powered, allowing for a two-wire circuit.
20 mA is considered an intrinsically safe signal in most locations.
Elimination of the voltage drop errors results from long wiring runs due to the constant-current feature of a current loop.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre