{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the PM5560 support a simultaneous EtherNet/IP and Modbus TCP connection?

Article available in these languages: Spanish

Issue
There is a need to communicate with a PM5560 series meter simultaneously with EtherNet/IP and Modbus TCP connections.

Product Line
PM5560 (METSEPM5560)
PM5563 (METSEPM5563)

Environment
Communication Protocols

Resolution
Yes, the PM5560 series meter can handle a simultaneous EtherNet/IP and Modbus TCP connection.

Note: The PM5500 supports EtherNet/IP as of firmware version 2.5.2.

Schneider Electric Saudi Arabia