{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Modbus Registers used by the Realflo flow computer in Realflo 7

When a Realflo flow computer is loaded and running in a SCADAPack controller, the flow computer reserves a range of Modbus registers for flow computer use only.  Modbus registers that are not being used by the flow computer may be used by the logic program.


The following tables illustrate which Modbus registers are reserved by the flow computer and which Modbus registers are available for use by the controller logic.


The same is true for the older ‘legacy’ SCADAPacks, the newer SCADAPack32 and SCADAPack 300 series controllers as well as for the newest SCADAPack x70 controllers.

Realflo Reserved Modbus Registers


The Realflo Flow Computer reserves the following hard-coded set of Modbus Registers.
Register Type5-Digit Addressing Range6-Digit Addressing Range
Discrete Coils3800 – 40963800 – 4096
Discrete InputsN/AN/A
Input Registers34000 – 39999304000 – 313999
Holding Registers42000 – 49999402000 – 411999


Realflo Registers Available for Users for standard SCADAPack Controllers


The following Modbus Registers are available for use with ladder logic programming.
Register Type5-Digit Addressing Range6-Digit Addressing Range
Discrete Coils00001 – 0379900001 – 03799
Discrete Inputs10001 - 1409610001 - 19999
Input Registers30001 – 33998 *300001 – 303998 *
Holding Registers40001 - 41998400001 – 401998


* For SCADAPack 32 and 3xx controllers (i.e. SP32, SP334, SP357, etc) the ‘Input Registers’ range is 30001 – 39999 and 300001 – 303998
For older SCADAPack controllers (i.e. SCADAPack,  SCADAPackLP, SCADAPack100, etc) the ‘Input Registers’ range is 30001 – 31024 and 300001 - 301024


Realflo Registers Available for Users for x70 Controllers


The following Modbus Registers are available for use with ladder logic programming.
Register Type5-Digit Addressing Range6-Digit Addressing Range
Discrete Coils00001 – 03799, 04097 - 0999900001 – 03799, 04097 - 09999
Discrete Inputs10001 - 1409610001 - 19999
Input Registers30001 – 33998300001 – 303998
Holding Registers40001 - 41998400001 – 401998, 412000-465536

Schneider Electric Saudi Arabia