{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How is calculated Power Factor on PowerTag Sensors ?

Power Factor PF = P/S -> This is the ratio of active power and apparent power.
PowerTag calculates the apparent power with the following method S = Irms * Urms
RMS value of current (and voltage) includes the harmonic content
=> As a consequence, harmonics in the current are taken into account with this method

As a result, the method used by PowerTag gives an Apparent Power greater than the one produced by Energy Meters like IEM2000 or iEM3000 series , and consequently a worse PF.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: