Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Profibus device Slot Configuration for a ifm10DBB profibus slave device is missing drop down list.
Issue
If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.

Product Line
PMEPXM0100

Environment
Windows 10

Resolution

If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.

The cause of the issue is due to the software failing to decode the gsd file when the allowable slot module range (“x-y”) starts with zero. (i.e. x = 0).

Note: There is no issue when the allowable modules are in a list e.g. 0,1,2,3,4… or if the module range does not start with zero, e.g. 1-5 or 100-115

To resolve the issue,
  • Open the .gsd file with Wordpad 
  • Locate the Slot(x) line for the slot that is having the problem.
  • Change the “Allowable Module Range from 0-4, to 0,1-4.  (See example below).
  • Save the changes.
  • Retest.

Change the “Allowable Module Range from 0-4, to 0,1-4.
From:
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0-4
To:
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0,1-4

 

Schneider Electric Saudi Arabia