{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How is Data Logging done on Altivar Process drives?

Issue:
Data Logging capability available on Process drives.

Product Line:
ATV600, ATV900, ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
Yes, Data Logging is available on  Process Drives.
The function gives the possibility to the customer to log up to 4 parameters distributions at the same time.
Each parameter storage is synchronized with a predefined sample time.
However, the Log has to be activated and deactivated as needed.
The result of this function gives the possibility to extract a bar graph with 10 bars (every 10% of the defined maximum value)
to visualize the distribution for each of the four selected parameters via SoMove or Web server.

Schneider Electric Saudi Arabia