Search FAQs
Can I add a delay timer on each ATS01 soft starter to avoid overloading the pumps?
Issue:
Can I set up a timer to start three soft starters in sequence?
Product Line:
Altistart ATS01
Environment:
All model numbers
Cause:
Customer want to start each soft starter in sequence using a timer delay.
Resolution:
Customer has to use external controls because it is not a feature of ATS01.
Can I set up a timer to start three soft starters in sequence?
Product Line:
Altistart ATS01
Environment:
All model numbers
Cause:
Customer want to start each soft starter in sequence using a timer delay.
Resolution:
Customer has to use external controls because it is not a feature of ATS01.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: