Search FAQs
How to upload a program with EcoStruxure Operator Terminal Expert 3.1 ?
Issue:
Unable to find any function to upload an application from an HMI running the EcoStruxure Operator Terminal Expert V3.1.
Product Line:
Vijeo XD 3.0, EcoStruxure Operator Terminal Expert V3.1, EcoStruxure Operator Terminal Expert V3.1 SP1
Resolution:
In the current version of EcoStruxure Operator Terminal Expert V3.1 SP1, there is no functionality to allow a user to upload an application from the HMI to be used on your PC to make edits or changes. Please be sure to backup your source file after your commissioning is complete.
Unable to find any function to upload an application from an HMI running the EcoStruxure Operator Terminal Expert V3.1.
Product Line:
Vijeo XD 3.0, EcoStruxure Operator Terminal Expert V3.1, EcoStruxure Operator Terminal Expert V3.1 SP1
Resolution:
In the current version of EcoStruxure Operator Terminal Expert V3.1 SP1, there is no functionality to allow a user to upload an application from the HMI to be used on your PC to make edits or changes. Please be sure to backup your source file after your commissioning is complete.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: