{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does PSO support OPCUA?
Issue
Although developed by the same organization, OPC UA differs significantly from its predecessor, Open Platform Communications (OPC). The Foundation's goal for OPC UA was to provide a path forward from the original OPC communications model that would better meet the emerging needs of industrial automation.

Product Line
Power SCADA Operation, PSO

Environment
OPC UA (OPC Unified Architecture)

Cause
Using this driver in PSO to communicate with some devices.

Resolution
This driver is supported at no additional cost. Driver version 3.01.05.000 is attached to this article.

OPCUA Driver Version History (included in the ZIP file):
3.01.04.000
2.03.09.000
1.20.00.000
1.20.00.001

Schneider Electric Saudi Arabia

Attachment(s)
OPCUA_3.01.05.000_RELEASE.zip [25.7 MB]