{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to use Profile Editor to add a device type to a Power SCADA Operation (PSO) project

Issue
A device needs to be added to a PSO project, but that device type is currently not included in that project.

Product Line
Power SCADA Operation 9.0

Power Operation 2021

EPO 2022
Environment
PSO Server, Profile Editor

Resolution

  1. Open the Power SCADA Studio application and Navigate to the Topology page. Open the Device Profile Editor located on the far right.
  2. If the device profile is already created, but not added to the project, click on the Set Up Projects tab. If the device profile is for a third party device, or is not already created, refer to FA404307
    for instructions on creating a device profile.
  3. Select the Project and click Add / Edit.
  4. Leave Edit Existing selected and verify the project name is correct. Find the device profile on the left hand side, highlight it, and click the arrow to move it over to the right hand side.
  5. Hit Save & Exit, then hit Export Project. The device profile is now added to the project and can be selected as a device type.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.