Issue:
Why can't I assign 2 compatible functions to the same digital input?
Product Line:
ATV630, ATV660 , ATV650
Environment:
All serial numbers ,
Cause:
Programming Hand Off Auto functionality
Resolution:
Need to verify that the Access Level is set to Expert. Then you can assign 2 different functions to the same digital input.
Why can't I assign 2 compatible functions to the same digital input?
Product Line:
ATV630, ATV660 , ATV650
Environment:
All serial numbers ,
Cause:
Programming Hand Off Auto functionality
Resolution:
Need to verify that the Access Level is set to Expert. Then you can assign 2 different functions to the same digital input.
Released for:Schneider Electric Saudi Arabia