{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PSO2020_Chinese installers interface display messy code
Issue
The issue is related to PSO2020 installation with Chinese version of Operating system. We follow the system guide with supported OS. But the installer displaying messy code during installation:
install messy code1
install messy code 2
Environment
EcoStruxure Power Operation (EPO) 2020

Cause
In the installer, the Chinese resource file have issue and it can’t be display correctly. This will likely not be addressed in the PSO 2020 ISO directly as that would require a rerelease.
Resolution
Please download the newest PSO 2020 R2 ISO installer which already fixed this issue.
Check the following link for details.
PSO 2020 R2 ISO (latest set of complete updates for PSO v2020 released  September 17, 2020)
  • Description: ISO installation media for Power SCADA Operation 2020 R2
Please check the following link in Exchange :
https://ecoxpert.se.com/de/search#documentUUID/317babcc-98b5-31c2-d702-cb19654954a2/PSO_2020_20260.02/tab/documents

Schneider Electric Saudi Arabia