Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert 9.0 - Creating a new ION_Data when CU2 has been applied.
Issue
On a PME 9.0 system with CU2 applied; if the Database Manager is used to create a new ION_Data database, the stored procedures
  1. dbo.CleanCorruptIncidentsAndAlarms is missing and
  2. dbo.ClearAllProcessedAlarmData is not up to date.
This potentially causes issues in processing events.

Product Line
Power Monitoring Expert 9.0

Environment
Power Monitoring Expert 9.0 CU2

Cause
Commulitavie updates 2 (CU2) for PME 9.0 adds the CleanCorruptIncidentsAndAlarms as a stored procedure and also updates the existing ClearAllProcessedAlarmData stored procedure. If the Database Manager (or PME reconfigure) is used to create a new ION_Data after applying CU2, dbo.CleanCorruptIncidentsAndAlarms stored procedure will be missing and dbo.ClearAllProcessedAlarmData will not be up to date.
The stored procedures can be found in SQL Server Management Studio (SSMS), expand Databases-->ION_Data-->Programability-->Stored Procedures

Resolution
In order to update the newly created ION_Data database, run the CU2 installer in Reconfigure mode using the following steps;
  1. Navigate to Program Files (x86)\Schneider Electric\Power Monitoring Expert\Uninst_PME 9.0 Cumulative Update 2.
  2. Right-click on Setup.exe and Run as Administrator.
  3. Select Reconfigure.

Schneider Electric Saudi Arabia

Power Monitoring Expert 9.0 - Creating a new ION_Data when CU2 has been applied.
Issue
On a PME 9.0 system with CU2 applied; if the Database Manager is used to create a new ION_Data database, the stored procedures
  1. dbo.CleanCorruptIncidentsAndAlarms is missing and
  2. dbo.ClearAllProcessedAlarmData is not up to date.
This potentially causes issues in processing events. 

Product Line
Power Monitoring Expert 9.0

Environment
Power Monitoring Expert 9.0 CU2

Cause
Commulitavie updates 2 (CU2) for PME 9.0 adds the CleanCorruptIncidentsAndAlarms as a stored procedure and also updates the existing ClearAllProcessedAlarmData stored procedure. If the Database Manager (or PME reconfigure) is used to create a new ION_Data after applying CU2, dbo.CleanCorruptIncidentsAndAlarms stored procedure will be missing and dbo.ClearAllProcessedAlarmData will not be up to date.
The stored procedures can be found in SQL Server Management Studio (SSMS), expand Databases-->ION_Data-->Programability-->Stored Procedures

Resolution
In order to update the newly created ION_Data database, run the CU2 installer in Reconfigure mode using the following steps;
  1. Navigate to Program Files (x86)\Schneider Electric\Power Monitoring Expert\Uninst_PME 9.0 Cumulative Update 2.
  2. Right-click on Setup.exe and Run as Administrator.
  3. Select Reconfigure.

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.