{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why am I not able to see my DFB private variables with the OPC UA module BMENUA0100?

Issue:
DFB private variables are not showing with the OPC UA module BMENUA0100


Product Line:
EcoStruxure Control Expert, Unity Pro, M580, OPC UA, BMENUA0100


Resolution:
In order for the OPC UA server to access the DFB private variables, it is necessary to select the option "Include DFB/PU private variables" in the unity project settings under the "PLC embedded data" section

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: