Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Why is my Mac OS not a supported system for PowerChute Personal Edition v3.1?

Issue:
Mac OS is not a supported Operating System

Product Line/s:
Back-UPS
PowerChute Personal Edition

Environment:
Mac OS X attached to APC Back-UPS via USB cable



Cause:
PowerChute Personal Edition software provides safe system shutdown in the event of an extended power outage and provides potential data corruption. Mac OS has this option available natively.

Solution:
You can configure native Energy Saver options in System Preferences. For assistance with Energy Saver options, please review Configuring native shutdown on Mac OS X. 

NOTE: PowerChute Personal Edition has been discontinued. 


 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: