{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Replacement of existing SPD910 Series Differential Pressure Switch ?
Schneider Electric has released an update to the existing SPD910 Series Differential Pressure Switch. Refer to the below table for the replacement of the old model. Process connections and electrical connections remain fully identical. Presets are unchanged and no changes have been made to the existing housing/packaging.

Specification Sheet:
SPD910 Differential Air Pressure Switch Specification Sheet

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: