{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the authorized online modifications of Control Expert?

Issue
Define the modifications that can be done on the application and not requires a "Rebuild All".

Product Line
Ecostruxure Control Expert

Environment
Control Expert v14.1, Windows 10 version 1902 (OS Build 18362.30)

Resolution
You can find below a spreadsheet with the online modifications allowed on EcoStruxure Control Expert.
im1
im2
im3

Schneider Electric Saudi Arabia