{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PME2020-French Diagrams/Vista show incorrect units for "Current"

Issue

When the language is set to “French” in the Web application settings, the unit for “Current” displayed in the diagrams or Vista is incorrect.
Instead of “A” is showing ‘1’.
The issue is not observed for any other language.


Environment

First observed in PME2020 when localization in WebApps is set to French


Cause
The translation setting in French for the ResourceKeyname is set to ‘1’ in the [Internationalization].[LocalizedStrings] table ApplicationModules Database
You can confirm the Localization string for this language by running the following script
USE [ApplicationModules]
GO

SELECT [Id]
,[LanguageSpecifier]
,[ResourceSetName]
,[ResourceKeyname]
,[LocalizedValue]
FROM [Internationalization].[LocalizedStrings]
where ([LanguageSpecifier] like 'fr') and ([ResourceKeyname] like 'a')
GO

If the output of the query returns "LocalizedValue" to '1', the system is affected by this issue.



Resolution
1. Backup all PME databases
2.Update the customer's system by running the following SQL script on their Application Modules database
EXEC [Internationalization].[WriteLocalizedString] 'fr', 'DiagramResources', '', 'a', '', N'A'
3.Restart the applications to see the change. It should look as below

Schneider Electric Saudi Arabia

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: