{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to connect Thermal Sensor TH110 to SCADA with Modbus TCP/IP?

The TH110 should be associated with a Zigbee concentrator such as ZBRN32,but this one has a Modbus Serial Line Communication .

Accordingly, and as per the attached drawing (Pages from AAM74807 Ind A.pdf) the ZBRN32 can be linked to a PLC. The PLC reads the data of the ZBRN32 (temperature given by TH110) and the PLC could communicate to the Scada by a TCP/IP link by Modbus protocol.

Schneider Electric Saudi Arabia