Configure PSO OPC Server, when running PSO runtime as service
Please see attached PDF to follow the steps required to configure OPC DA Server when running PSO runtime as service. Applicable to PSO versions, 8.2, 9.0 and 2020
Released for:Schneider Electric Saudi Arabia
Attachment(s)
FAQ_OPC as Service.pdf [669.13 KB]
Explore more
Range:
EcoStruxure™ Power SCADA Operation 8.2
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.