{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is my Speed D Switchboard rated 80% or 100%

The Class 2710 Speed D Switchboard is rated for 80% of it maxi um rating or Over Current Protective Device (OCPD). Currently there is not an option for a 100% rated Speed D Switchboard.

For a 100% rated Switchboard application a Power-StyleTM QED-2 Series Switchboard will need to be considered.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: