Issue:
Can I program drive to switch between different set points on PID controller for the ATV630 drive?
Product Line:
ATV630
Environment:
All models, all serial numbers
Cause:
Customer wanted to easily switch between three set points, 40, 60 and 80 PSI.
Resolution:
Under the main menu, enter complete setting -> Pump Functions -> PID Controller -> PID Reference -> PID preset references:
Assign a digital input (DI5) for 2 PID Preset Assign
Enter 40PSI for RefPID Preset 2
Assign a digital input (DI6) for 4 PID Preset Assign
Enter 60PSI for RefPID Preset 3
Enter 80PSI for RefPID Preset 4
Note: This function can be accessed if [PID feedback ass.] PIF is assigned.
Can I program drive to switch between different set points on PID controller for the ATV630 drive?
Product Line:
ATV630
Environment:
All models, all serial numbers
Cause:
Customer wanted to easily switch between three set points, 40, 60 and 80 PSI.
Resolution:
Under the main menu, enter complete setting -> Pump Functions -> PID Controller -> PID Reference -> PID preset references:
Assign a digital input (DI5) for 2 PID Preset Assign
Enter 40PSI for RefPID Preset 2
Assign a digital input (DI6) for 4 PID Preset Assign
Enter 60PSI for RefPID Preset 3
Enter 80PSI for RefPID Preset 4
Note: This function can be accessed if [PID feedback ass.] PIF is assigned.
Released for:Schneider Electric Saudi Arabia