{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert v8.2: KPI Report missing calculated data when input sources have different Data Interval and one has Time Jitter
Issue
Azzo Calculation Engine Report is not handling the rollup properly if there is time jitter.

This issue is observed in the PME v8.2 system running KPI reports in which if out of two devices one has time jitter and both devices are logging in different time interval (for Ex: one logging with 15min and another with 30min)




Environment
PME 8.2 with Azzo Calculation Engine.

Cause
Issue with the Azzo Calculation Engine report logic.


Resolution
To fix this issue, download the attached 'PME8.2_KPI-ReportingHotFix.zip' contains 'Reporting.AZZO.Common.dll' file, unzip the same and replace the file in the PME install directory ‘\system\ReportDataService\bin’ folder.

Schneider Electric Saudi Arabia

Attachment(s)
PME8.2_KPI-ReportingHotFix.zip [11.25 KB]