{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Unable to download to HMISTO7 over USB cable with Virtual Machine

Issue:
Download over USB cable fails to start when using a Virtual Machine (VMware, Fusion, etc) running EcoStruxure Operator Terminal Expert

Product Line:
HMISTO, HMIGTU, HMIST, EcoStruxure Operator Terminal Expert

Resolution:
When running EcoStruxure Operator Terminal Expert in a Virtual Machine (VMWare, Fusion, etc), ensure to set the USB Compatibility to version 1.1 if you require to download to the HMI via USB cable. If you leave it at 3.0 or 2.0, the USB download will not start.


Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: