Search FAQs
What versions of Vijeo Designer are supported for EcoStruxure Machine Expert?
Issue
What versions of Vijeo Designer are supported for EcoStruxure Machine Expert v1.0, v1.1 , v1.2.0 and v1.2.2?
Product Line
EcoStruxure Machine Expert, Vijeo Designer
Environment
PLC/ HMI Configuration software on Windows PC
Resolution
See the table below for supported Vijeo Designer versions on EcoStruxure Machine Expert v1.0 and above:
Notes:
What versions of Vijeo Designer are supported for EcoStruxure Machine Expert v1.0, v1.1 , v1.2.0 and v1.2.2?
Product Line
EcoStruxure Machine Expert, Vijeo Designer
Environment
PLC/ HMI Configuration software on Windows PC
Resolution
See the table below for supported Vijeo Designer versions on EcoStruxure Machine Expert v1.0 and above:
EcoStruxure Machine Expert version | Vijeo Designer version that is included with install |
v1.0 | Vijeo Designer is not included |
v1.1 | v6.2.8.1016 |
v1.2.0 | v6.2.9.1008 |
v1.2.2 | v6.2.9.1008 |
Notes:
- EcoStruxure Machine Expert v1.0 was only for PLC configuration and did not include HMI devices in the Logic Builder component. You will need a minimum of EcoStruxure Machine Expert v1.1 to include Vijeo Designer and the HMI devices in the Logic Builder.
- As of this time of this FAQ's writing (May 2020), there are no additional Vijeo Designer Service Packs published for the above versions.
However, future Vijeo Designer Service Packs may be found in the Schneider Electric Software Update Tool launched from the Windows Start -> Programs -> Schneider Electric -> Software Update -> Software Update (shortcut icon)"
- It is recommended that only one version of EcoStruxure Machine Expert (or SoMachine) be installed on one Windows PC at a time.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: