{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to connect the wiring to HMIPSPS742D1001 COM2 for RS485 Modbus RTU communication
  1. Issue
How to connect the wiring to HMIPSPS742D1001 COM2 for RS485 Modbus RTU communication.
  1. Environment
HMIPSPS742D1001.
  1. Resolution
HMIPSPS742D1001 is a product of Easy Harmony Panel iPC. The port definition of HMIPSPS742D1001 is different with HMIPSP S-Panel PCs, so user can’t refer to the manual of HMIPSP S-Panel PCs.
Here is the Pin connection of HMIPSPS742D1001 COM2, user can connect to Pin 3 and Pin7 for RS485 Modbus Rtu communication.


  1. FAQ Applicable Conditions
FAQ applies to HMIPSPS742D1001.

Schneider Electric Saudi Arabia