{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to perform a factory reset on SmartX IP Controller devices?

Issue:
Steps for SmartX IP controller devices (MP-C, MP-V, IP-IO, RP-C).

Product Line:
EcoStruxure Building Operation, SmartX IP controller devices

Resolution:
In WorkStation, if your SmartX IP controller device seems completely unresponsive, perform a factory reset to restore the device to a state where it can be successfully commissioned. After you release the reset button, a factory reset may take up to 30 seconds to process. All diagnostic logs and the database are erased during a factory reset. By contrast, controller firmware does not revert and remains at the same active level.
To perform a factory reset using the hardware reset button, press and hold the reset button for 20 to 29 seconds. If MP-C or IP-IO is equipped with the MP-C Display add-on module, a count-up timer and progress bar are displayed to assist in reset selection. There is also a reset mode indicator that lets you know which reset occurs if you release at that time.
The below figures show the location of the reset button on different SmartX controller devices:
Location of reset button on MP series controllers
Location of reset button on IP-IO module Location of reset button on RP series controllers
Note: From EcoStruxure Building Operation v3.1+, there is a facility to remotely Factory Reset a SmartX IP Controller device, check below KB article for more information: https://community.exchange.se.com/t5/Building-Automation-Knowledge/Remote-Factory-Reset-of-SmartX-IP-controller-MPX-RPC-IPIO/ta-p/195345

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.