{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a PM2000 or PM5000 series meter operate above 2000m?
Issue:
Its not mentioned whether these power meters can operate at altitued higher than 2000m.

Environment:
EasyLogic™ PM2000 series
PowerLogic™ PM5000 series

Resolution:
We are not recommending either of these devices to use above it's specified altitude. During our testing, we have noticed some issues with creepage and clearance requirements when it is used above 2000m altitude.

Schneider Electric Saudi Arabia