Issue
The BMXDRA0815 modules 3.3V Power Budget is incorrect in Control Expert 14 and 14.1.
Product Line
M580
BMXDRA0815
Resolution
The correct 3.3V Power Budget for a BMXDRA0815 is 40ma.
It is incorrectly calculated and displayed as 100ma in CE14 and 14.1.
This issue is corrected in Control Expert version 15.
The BMXDRA0815 modules 3.3V Power Budget is incorrect in Control Expert 14 and 14.1.
Product Line
M580
BMXDRA0815
Resolution
The correct 3.3V Power Budget for a BMXDRA0815 is 40ma.
It is incorrectly calculated and displayed as 100ma in CE14 and 14.1.
This issue is corrected in Control Expert version 15.
Released for:Schneider Electric Saudi Arabia