{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Lighting calculation for Lighting Kit part numbers; ACDC2018, ACDC2019

Can Schneider Electric provide lighting calculation files (.ies)? The customer is trying figure out a way to show adherence to our standards with the lighting used in the containment units. We have to have a minimum of 50 foot candles at all racks/cabinets.

Schneider-Electric does not provide such .ies files, however attached is the photometric specs needed.  The document gives the footcandles at various locations.  Note that if frosted lens are used, a .75 multiplier must be applied. There are qty 4 in the ACDC2018, qty 6 in the ACDC2019

Schneider Electric Saudi Arabia

Attachment(s)

ACDC201X Lights.pdfACDC201X Lights.pdf [47.01 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: