{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can your wire up an HOA on a ATV212 drive?
Issue:
HOA wiring and programming for ATV212 drives.

Product Line:
ATV212

Environment:
All

Cause:
programming and wiring HOA switch

Resolution:

RES is wired for HOA and (HO) is low and (A) is high

POT is wired to VIB PP and CC
4-20ma is wired to VIA and CC

FNOD-2 VIB or POT
F207= VIA or 4-20mA signal
F113 - RES program = 38 for auto manual.

Schneider Electric Saudi Arabia