{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the BMXERT1604T be synchronized without IRIG-B and DCF77 source in a M580 project ?

1.Issue

Can the BMXERT1604T be synchronized without IRIG-B and DCF77 source in a M580 project ?

2.Environment

M580 series

3.Resolution

The BMXERT1604T with Firmware version >=SV2.0 could be synchronized by M580 Standalone CPU via Xbus by selecting CPU/CRA head as externel clock source.
User needs to select BMXERT1604.2 during hardware configuration .

The clock sync source needs to be CPU/CRA head




Detailed compatibility matrix is shown as below






Schneider Electric Saudi Arabia